PLUS+1 Software > Displays
DP610 colour issues
(1/1)
Richard:
I'm having trouble with the colours changing a bmp. I'll create a simple bitmap, add it to the library in the screen editor and it changes colour immediately, on other occasions it waits until I drag it in to a screen before screwing up. On others I'll have to exit the screen and then it changes on re-entry.
I've checked the obvious, it's 8 bit, I've recreated it using different software, it uses the pallette from the bmp, I've deleted it and created another with a different name. The colour changes from a shade of orange to yellow and the simulator shows the same problem so does a real DP610. The software I'm using it not new, I used it for countless other bmp before and after with no problems.
Any ideas or work arounds?
Richard
Thomas:
Hi Richard!
This was a odd one, please send it to helpdesk@sauer-danfoss-plus1.com because this is something we need to look closer at.
Sorry for your troubles // Thomas
Quax76:
I also have some troubles with the colours, since using V5...
1. When I open a project created with v4.x the texts on a screen area aren't black. It seems, that they are a kind of brown... (see image). On the Display, the colours are OK.
2. The next issue is to control the colour of a bitmap. In versions earlier than 5, I was able to change the colour of a b/w bitmap by using a signal. In the new Plus1, the change has no effect. The image is still black.
Navigation
[0] Message Index
Go to full version