Hi Acmall and Tor,
Thanks for your message
Now I can see 0, 28 option in ECU list.
So I flashed a new program without any changes into it and I can see both option (0, 27) and (0, 28). Still even I flashed both program, I can not see any output at pin 34 and 46. (I set the Digout to "True" before flashing it).
I investigated little more and the behavior of yellow LED is constantly HIGH. Even after flashing both the controller. I read it that it means it is "activated for Safety layer in error conditions"
No RED LED so it means no CAN fault. I think LED should be in GREEN mode then it should work correctly. (Correct me if I am wrong). Any help how to resolve those error conditions?
For the other devices connection, no its just Danfoss controller connected with the power supply. No other connection.
"For the attachment issue, I feel that the image size should not be large enough. If it is, page does not refresh and actual message failed to post.