PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: bryantmorris on September 07, 2015, 01:03:50 PM
-
Hello,
Is there anyway to measure the operating temperature of the MC050-110. I can't see any system variables in Plus+1 that allow me to measure the temperature ie in the same way I measure system voltage etc. I don't need any specific place, just somewhere on the inside of the controller.
Is there anyway I can get access to this information or is it not physically built into the controller.
Thanks in advance.
-
Hello,
as far as I know, there is no possibility to read out the temperature from the Controller.
Am I allowed to ask, why you need this value ?
Best regards
FStelzer
-
Thank you for the feedback.
With my systems I try to relay as much information to a display to help with fault monitoring. When I use other hardware I include the operating temperature of any of the units connected to the CAN bus. I would have liked to have done the same thing with the PLUS+1 units.
-
Hello,
as I said in the last post, there is no possibility to read out the operating temerature from a Controller, Display or an IO module.
You can read out the operating temperature on a H1AC pump or digital magnets (PVED CC, PVED CX , PVEA CI, PVEO CI) . There is a possibilty to read out the PCB temperature of these components. I don't know if you have installed one of these components.
Otherwise you have to find out any other solution to get the operating temperature.
KR,
FStelzer
-
Hi, FStelzer in DP200 is possible!! I never use it but in Inputs/OS it is present!
Bye ;)
-
Thanks I should survive for this application.
Just take note that other product on the market includes features like this.