Author Topic: Compiling with SSA Blocks in program  (Read 9310 times)

Nick Anderson

  • Guest
Compiling with SSA Blocks in program
« on: April 19, 2012, 02:05:14 AM »
I am trying to compile using the Fan Drive SSA block, and I continue to get an error saying *** ERROR 309 *** [CHPARGU1] APPLICATION BLOCK IS LOCKED TO HARDWARE {10106603}.  Reading through some things, it looks like you have to have keyed hardware in order to load a program containing an SSA onto the controller, but there shouldn't be a restriction on compiling it to create your downloadable file, right?  All help is appreciated.

Offline Slashe

  • PLUS+1 Novice
  • *
  • Posts: 4
  • Karma: +0/-0
Re: Compiling with SSA Blocks in program
« Reply #1 on: April 19, 2012, 08:30:53 AM »
Hi Nick!

You should try this. There is a place for Target part number in the project manager tab in the GUIDE. You should try to enter the number (10106603) there and then try to compile.

Slashe