Author Topic: CAN-Be-Safe CRC Algorithm  (Read 7183 times)

carlson.john

  • Guest
CAN-Be-Safe CRC Algorithm
« on: January 07, 2015, 06:03:22 PM »
Is there a specified PLUS+1 Standard CRC Algorithm with supporting source code?
I am dealing with a couple of devices from different manufacturers.  One device has implemented CAN-Be-Safe data transmission described in the PLUS+1 Safety Message White Paper.  Another device attempts to validate the SDM CRC with the SDH message using the C86C Polynomial in the White Paper.  The CRC's do not match.
Am I correct in stating that, if the two manufacturers do not use identical CRC implementations, they will never be able to successfully utilize CAN-Be-Safe?
If that assumption is true, then how does an OEM that needs equipment from several different device makers integrate the various devices?