Author Topic: Sauer-Danfoss CG150 cable and codesys  (Read 7178 times)

Offline ripplingwater

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
Sauer-Danfoss CG150 cable and codesys
« on: November 13, 2017, 03:54:14 PM »
hi,

I have a Sauer-Danfoss CG150 CAN to USB cable ( image attached ) and I was trying to connect an Connector Interface Board ( connected to an ECU ) to CODESYS 2.3. The earlier cable used was a PEAK CAN Cable that I am not really sure of but then I was wondering the comm settings when using Sauer-Danfoss CG150 cable. The rest of the settings are default ECU comm settings and should be fine but there is one field called "CAN card driver". I was wondering what is the value to use for that? I have attached a screenshot. Many thanks

Screenshot:https://imgur.com/a/nmzmQ


Cheers,
RW