Author Topic: Vertical text  (Read 11806 times)

Offline jashom1

  • PLUS+1 Expert
  • ****
  • Posts: 78
  • Karma: +6/-0
Vertical text
« on: February 10, 2016, 12:29:38 AM »
Hey gurus,

If someone was to use the Monitor (say DP700) in a portrait orientation, this would need the ability to rotate the text fields 90°

Without rendering the text to an image and rotating that, I can't see how this can be done.  It would be nice to have a rotation field on the text boxes, you could then create some cool rotation effects  :)

Cheers.

John.

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Vertical text
« Reply #1 on: February 11, 2016, 08:34:37 AM »
Hello John

To use the DP700 in a portrait orientation, Do the following:
1)   Make sure that you are using a recent HWD for your DP700 display (in this example version 140 was used)
2)   Select the ScreenDef
3)   In the inspector, select a Rotation value of 90 (or 270) degrees
4)   Add texts to your screens as you normally would, see attached example screenshot.


Best regards
Daniel
PLUS+1® Help desk
PLUS+1® Help Desk Team

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Vertical text
« Reply #2 on: February 11, 2016, 09:02:47 AM »
Very nice.
In classic screen editor (DP610TM) not possible?
OK, I don't need this feature.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline jashom1

  • PLUS+1 Expert
  • ****
  • Posts: 78
  • Karma: +6/-0
Re: Vertical text
« Reply #3 on: February 16, 2016, 02:26:14 AM »
Ahh!

Thanks Daniel :)

John.

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Vertical text
« Reply #4 on: August 07, 2017, 01:56:50 PM »
Is it also possible to have a normal landscape orientation and one text is rotated to 90° ?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: Vertical text
« Reply #5 on: November 06, 2017, 12:58:55 PM »
Hi Marbek!

I'm sorry but we don't support rotation of texts. In that case you'll have to use a image of the text which is possible to rotate.

Best regards
Nilla
PLUS+1 Helpdesk team

Offline Remy

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +0/-0
Re: Vertical text
« Reply #6 on: March 28, 2018, 07:37:01 PM »
Is it also possible to have a normal landscape orientation and one text is rotated to 90° ?

I've never done it, but you could easily create a widget with your text being a screen definition with a 90º rotation and integrate it to your normal screen

Offline Kava_Man

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
    • LIVE Magazine
Re: Vertical text
« Reply #7 on: March 11, 2019, 11:13:32 AM »
Hello John

To use the DP700 in a portrait orientation, Do the following:
1)   Make sure that you are using a recent HWD for your DP700 display (in this example version 140 was used)
2)   Select the ScreenDef
3)   In the inspector, select a Rotation value of 90 (or 270) degrees
4)   Add texts to your screens as you normally would, see attached example screenshot.


I wish more replies were this concise. I particularly appreciate the screenshot - makes things a lot easier for people like me. Thanks for taking the time to post!