PLUS+1 User Forum

PLUS+1 Hardware => Displays => Topic started by: Quax76 on November 05, 2010, 11:42:53 AM

Title: USB stick on display?
Post by: Quax76 on November 05, 2010, 11:42:53 AM
Hi everybody,

is there a chance to connect an usb-stick to one of the available displays to write machine configuration data on it?
What I would like most is to use DP610 and connect a USB connector to the 7 pin Binder connector (C3).
If this doesn't work, could I use the DP210 with front USB (using application data kogging)?

Thanx!
Title: Re: USB stick on display?
Post by: Stefan on November 09, 2010, 11:18:55 AM
Hello,

There are plans to implement components that can extract the data from an Application logg and send it to the USB-port but it's not available yet. Unfortunately I can give you any date when it will be released.

Stefan