Author Topic: Define Areas Page and the Define Screen Page  (Read 931 times)

Offline Daan

  • PLUS+1 Developer
  • ***
  • Posts: 23
  • Karma: +1/-0
Define Areas Page and the Define Screen Page
« on: March 15, 2023, 03:51:16 PM »
Hello

I wanted to start programming/creating my display using Define Areas Page and the Define Screen Page but these are no longer in Display.
Where could I find these?

Thank you in advance
Junior Mechanical Engineer

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Re: Define Areas Page and the Define Screen Page
« Reply #1 on: March 16, 2023, 08:49:02 AM »
There are two different screen editors, the Classic Screen Editor is used for the older displays and the Vector Based Screen Editor (VBSE) is used for the newer ones. It looks like you are using one of the newer displays that uses the VBSE in which case Define Areas Page and the Define Screen Page are not used, the screen is displayed using the Show Screen Component.

Offline Daan

  • PLUS+1 Developer
  • ***
  • Posts: 23
  • Karma: +1/-0
Re: Define Areas Page and the Define Screen Page
« Reply #2 on: March 16, 2023, 10:11:36 AM »
Thank you!
Junior Mechanical Engineer