PLUS+1 Tools > PLUS+1 Service Tool
File Download Failed
(1/1)
williamk:
Occasionally I will get an error with the text: "Error: Download transfer timeout" and Download Status: "E266: Download transfer timeout".
Is there some way to increase the timeout? I've seen this error while using a PEAK adapter in RP1210C mode and while using a Kvaser Leaf Light. In both instances, the display (DM430E) and the adapter were the only things connected to the CAN bus and the bus had proper terminating resistors.
vnikola:
Hello!
Have you found the solution to this problem, as we are experiencing almost the same thing here.
Regards,
Nikola.
Fredrick:
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.
Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is buggy.
sverreo:
--- Quote from: Fredrick on June 08, 2023, 05:48:30 PM ---I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.
Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is glitchy.
--- End quote ---
Fredrick, what do you mean CAN-King is glitchy?
Fredrick:
Ok, maybe I used the wrong word for it ;)
CAN-King does not work for me, the program freezes or stops behaving normally after a while.
PCAN View always works and you can use both ServiceTool and PCAN View at the same time.
Yes, I know that you can do that with CAN-King as well if you configure it right.
Navigation
[0] Message Index
Go to full version