Author Topic: Congratulations for PLUS1 Update Center  (Read 9195 times)

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 116
  • Karma: +6/-1
Congratulations for PLUS1 Update Center
« on: July 19, 2017, 09:09:51 PM »
Hi,

I just updated from PLUS1 GUIDE 9.0 to 9.1 and I tried the new PLUS1 Update Center and I must say that it's a very nice tool. It will be a time saver for me as I'm using 3 different computers for PLUS1 programming and maintaining all the Hardwares Blocks up to date was a pain. Now, everything is easy.

Congratulations for such a nice addition!

Have a good day!

Sam

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 325
  • Karma: +7/-0
    • Marbek Elektronik
Re: Congratulations for PLUS1 Update Center
« Reply #1 on: July 20, 2017, 08:14:36 AM »
Are this the same hardware blocks as I can manually download?

I don*t want to change hardware block in a project.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 116
  • Karma: +6/-1
Re: Congratulations for PLUS1 Update Center
« Reply #2 on: July 21, 2017, 03:22:19 PM »
It won't change the hardware block already used in a project.

But, it will keep everything that is under the "Function" tab and the "Hardware" tab up to date. No more need to download anything from these webpage and then install them manually :

http://powersolutions.danfoss.com/products/plus-1-software/plus-1-microcontroller--hwd-files/#/
http://powersolutions.danfoss.com/products/plus-1-software/plus-1-compliance/#/
http://powersolutions.danfoss.com/products/plus-1-software/plus-1-function-block-library/#/

Also, it will keep the GUIDE and ServiceTool software up to date.

A very nice tool!

Sam