PLUS+1 User Forum
PLUS+1 Software => Displays => Topic started by: FST on March 16, 2011, 10:29:35 AM
-
My problem is, that if the value in the display are changing the position also will change.
With %5d the value will move on both side.
With %d the value will move to the rigth.
I saw in the DP200 with the EIC that there are value which are moving to the left.
How can I implement, that my value is fixed on the right an if I rise the value it will move the the left.
Thank you for your help.
Frank
-
You need to have Monotype fonts (same width on all letters and numbers) on the value you want to show and use %5d.
In DP200 program Sauer-Danfoss is using Aero-font for the text and fixed Aero font (monotype) on the values.
-
But I have used Aero Font and it is not Fixed size !?
Bernd
-
Hi there.
If you use %05d the units not in use will be filled with zeros such as 0017.
This will at least stop the fonts jumping around.
regards Neil.
-
Try using %-5d, That should left justify the number.
John.
-
Hi,
which fonts are you using (fixed size)?
It would be nice, to be able to right justify letters.
By,
Bernd