« Last post by Lukey on October 26, 2023, 02:44:11 AM »
I did not try constants instead of autotypes, as I found out with the assistance of Ryan from Help Desk that I was addressing input from an expansion module which do not have the HW "Per." capabilities for the FB to work correctly.
Tip for young players, read/plan carefully the pin requirements of the hardware FB prior to selecting the hardware.
« Last post by Lukey on October 26, 2023, 02:39:54 AM »
I can't comment from personally experience but the first thing that comes to mind; In your SC GUIDE program have you changed the CAN address for the Expansion Module to CAN 1 ? as default is CAN 0 I believe.
« Last post by macbahi on October 25, 2023, 09:50:57 PM »
Hello, I usually use SC050 ou SC024 CAN0 with module OX024-110 Can0. It's work very well. But now I am changing my communication with CAN1. So I can not see my module OX024 -110. Please the CAN+ CAN- of module OX024-110 can be CAN0 and CAN1. Or only CAN0.
« Last post by Camox on October 23, 2023, 10:34:30 AM »
Hello, We work with my colleagues on a network folder where our programs are stored. This allows us to easily share files, make backups... Since the last update of the Guide, 2023.3.3.5531, it is impossible to compile a program located in a network folder:
Hi all, i was wondering if there is a fast and easy way to draw lines and points dinamically. I have an array that defines a number of points (0 to 4096) and i wish to draw as points as the array length is. I can do this easily in other developement platforms (java,codesys,QT etc) but seems that is not possible to do it in GUIDE. i should to populate all 4096 elements in screen editor and them manage them manually??? . It' a huge work to do something that i can do in fwe lines of code in other dev envitonment. I hope i'm wrong...
« Last post by G30RG3 on October 19, 2023, 06:55:11 PM »
AFAIK the PVE should generate an error after 250ms. I guess you've set the fault monitoring to passive? Setting this to active, should bring the PVE to a safe state in case of an error.
« Last post by jert on October 18, 2023, 09:44:55 PM »
I have had a failure with our Danfoss PVED-CC S7 valves when the CAN network fails. If the valve was commanded on it keeps going even though the CAN network is down. Is there a parameter that I can set so that if the valve loses the CAN signal it will stop immediately or go to neutral?
This website uses cookies
We and our partners use technologies, including cookies, to collect information about you for various purposes, including:
Functionality, Statistics, Marketing
By clicking 'Accept All' you consent to all these purposes. You can also choose to indicate what purposes you will consent to using the [Check boxes], then press 'Update consent'.
You can always withdraw your consent by [clicking the small icon in the lower left corner of the page].
Detailed cookie information cannot be displayed if a cookie has been set behind a log-in webpage. However, the provided cookie consent prior to a log-in webpage is still applicable.
You can read more about our use of cookies and other technologies, as well as our collection and processing of personal data by clicking on the link.
Learn more