Author Topic: Please add basic drawing functionality  (Read 9108 times)

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Please add basic drawing functionality
« on: September 06, 2014, 12:58:51 AM »
I want to be able to make circles and rectangles.  Do I really have to draw basic shapes in my free Paint program and then import them into the (not free) industrial display program?  And if I want a shape in a slightly different color...I have to draw another image and import that.  This was probably the norm 20 years ago, but of the several brands of displays I've programmed in my time they all have had basic drawing capabilities.

You guys put in the ability to draw lines.  Why not other shapes?

I'm using the Vector Based Screen Editor which I think is the newer one.
Controls Engineer
Hydra-Power Systems

Offline bfpmark

  • PLUS+1 User
  • **
  • Posts: 6
  • Karma: +0/-0
Re: Please add basic drawing functionality
« Reply #1 on: February 24, 2015, 06:38:02 PM »
I agree with this request.  A triangle and circle would be nice.  Especially if you can control them with signals.  A third thing would be a pie (a circle with a missing wedge) where you could control the diameter of the circle and the angle of the missing slice both with parameters.

Offline ZanInno

  • PLUS+1 Developer
  • ***
  • Posts: 17
  • Karma: +3/-0
Re: Please add basic drawing functionality
« Reply #2 on: February 25, 2015, 04:03:08 AM »
I agree - There is lots of room for improvement.  Even circles and arcs would be helpful.

The being said, it is easy to create squares and triangles with individual lines, then control the size and location of the shapes with variables in the program.

The line width can also be set to any width - This can be used as a rectangle.  I have used this before to indicate a tank level.  By drawing a thick line over a tank graphic, it can represent the fluid level.  Variables in the logic control the line length.  Variables can also be used to change the color of the line(when the tank level gets low, line turns red).



Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Please add basic drawing functionality
« Reply #3 on: November 21, 2015, 08:24:27 AM »
And also add copy functionality :
copy in one screen page objects and paste them into another!
And: copy formattings in one page and format another objects by clicking with left mouse key, like in word or excel.

It is too much work to format text manually.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Please add basic drawing functionality
« Reply #4 on: December 22, 2015, 08:46:07 AM »
Hello Danfoss,

please make a few changes to "old" classic screen editor, because there are many new Displays, DP610TM, which work with this editor.

My wishes to this are:

- make possible to change the ID of a text object, because we want to copy screen from one program to another and so IDs have to be the same.

- copy and paste must be possible: in the same screen and from one screen to another screen

- copy formatting style must be possible in screen editor, like word and excel

- right formatting values must be possible


This are very helpfull and important functions. Please realize them! - Thanks in advance!
« Last Edit: December 22, 2015, 10:13:01 AM by Marbek_Elektronik »
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Please add basic drawing functionality
« Reply #5 on: April 27, 2017, 02:08:04 PM »
Hi,
now it ist 2017-04-27 and only 2 points are released in new vector editor:
- right formatting values must be possible
- copy and paste must be possible: in the same screen and from one screen to another screen

I think the 2 other points are not released in new vector editor:

- make possible to change the ID of a text object, because we want to copy screen from one program to another and so IDs have to be the same.

- copy formatting style must be possible in screen editor, like word and excel
It could be as folowing:
Select one Text,
then klick in an opening checkbox which proberties you want to copy (font size, style, but not position,...)
then klick the other texts you want to change.

This tool would save about 50% of time !
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Please add basic drawing functionality
« Reply #6 on: January 06, 2024, 02:14:50 PM »
Please release circles drawing, as basic function, again

If I use svg pictures and change size, the thickness of line will also change.

Basick drawings like lines, circles, rectangles and so on, woud bi nice.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Please add basic drawing functionality
« Reply #7 on: January 07, 2024, 11:56:13 PM »
You can do this already. Add>>Text/Vector Graphics>>Hollow Circle. Also from the side bar (see attached)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Please add basic drawing functionality
« Reply #8 on: January 09, 2024, 02:19:13 PM »
Hi,
thanks,
but I mean in screen editor. There es only one element: "line"
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Please add basic drawing functionality
« Reply #9 on: January 10, 2024, 04:56:10 AM »
oops sorry, i didn't read the whole thread.

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Please add basic drawing functionality
« Reply #10 on: January 16, 2024, 01:42:15 PM »
Hello again,
another basic drawing function: transparency %

Is it possible to overlay 2 pictures and to show both?
One 70% and the other 30% ?

We want to show a logo behinde every screen.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung