PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: metalninjadragon on October 28, 2014, 06:44:24 PM
-
I'm looking for a controller that can handle both profinet (industrial ethernet) and CAN J1939, to "bridge the gap" as it were between the industrial and off-highway world.
Is there any way to do this with a Danfoss controller?
-
Sure, knowing that J1939 is just a protocol overtop of CAN, just get one of the many CAN-to-Profibus converters or gateways out there, wire it up to the CAN output of the Danfoss controller, and you're done. At least, that's what the brochure says...
-
I guess you have already figure out what to do.
but just in case.
I had to get data from J1939 and RS485 to be shown in a DP600 (which only has CAN), what I learn is the following
1.- it makes things much easier if you understand both protocols (I had few knowledge of RS485)
2.- not all gateways are easy to set it up
3.- the gateways are designed for industrial aplications not for off road so they are more vulnerables to faliure in the field. of course you need a box to hold it.
I took me a couple of months to get it working becuase of my lack of knowledge in RS485, I ended up with a EATON gateway that works just fine (with this one you have to write down the RS485 code in C++) you can check the ADFweb ones it is supposed they are easy to set it up I was not able to get it working.
hope this hepls