Author Topic: Generate Read Only Parameter File  (Read 3421 times)

Folkert

  • Guest
Generate Read Only Parameter File
« on: April 25, 2013, 11:14:46 AM »
Hello,

Does anyone know if the "Generate Read Only Parameter File" tool inside Guide, can be called externally? I want to make an end of line tool with creating ROP files with an other tool.

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: Generate Read Only Parameter File
« Reply #1 on: April 25, 2013, 09:24:29 PM »
Hi Folkert.

I'm not sure of the "other tool" you of thinking of? I have used a small DP2XX display as a service tool to read and write to EE's and also to log info.
I included a extra 12 pin connector on the BUS. I really wanted to avoid starting up a laptop, connecting a CG150 etc.

The EE have a Boolean read and write function for this purpose.

regards Neil