Author Topic: Feature Request - Custom Enumeration Constants  (Read 2466 times)

Offline BrianF

  • PLUS+1 Developer
  • ***
  • Posts: 15
  • Karma: +0/-0
Feature Request - Custom Enumeration Constants
« on: August 11, 2022, 06:49:48 PM »
It would be very nice to have a way to create Custom Enumeration Constants.   Right now the software has an enumeration for the "Time Base."  The custom enumeration could behave similar to that feature.  Just make it a different color boarder to indicate that it is a custom enumeration constant. The base data type could be selected (U8, S16 etc.) so the data could pass through other built in components.

Thank you,
Brian F.