Author Topic: Download time in DM1000  (Read 3185 times)

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
Download time in DM1000
« on: September 06, 2022, 04:44:15 PM »
Hello,
I work actually on software for DM1000 dysplay.
The download time for add a software in the dysplay in long. During the download the load speed on the dyspaly is 10kb/s.

We can change the load speed ?

Thank in in advance.

Good day

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: Download time in DM1000
« Reply #1 on: September 07, 2022, 07:29:18 AM »
Hello Camox,

Yes the download time for the DM1x00 displays are a bit longer than the rest of units. Especially when you are replacing the HWD file and OS.
I recommend to use USB when working with the DM1x00 displays. You will save a lot of time. When it take almost an hour downloading a new OS with CG150, it will only take a minute with the USB.

If you want to order you can find the part number in the image below (11231512). You can also find it in the Data Sheet.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
Re: Download time in DM1000
« Reply #2 on: September 07, 2022, 08:05:11 AM »
Hello Thor,
Thank a lot four your response.

I’ll get that cable fast.

Have a nice day

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
Re: Download time in DM1000
« Reply #3 on: October 24, 2022, 03:22:14 PM »
Hello Thor,
Is it necessary to have a driver that the cable connection works?
Thanks

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: Download time in DM1000
« Reply #4 on: October 25, 2022, 09:01:03 AM »
Hello,

No, the drivers are included in the PLUS+1 Service Tool.
You need to use the Interlink Gateway.  See Image.

Have a nice day
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
Re: Download time in DM1000
« Reply #5 on: October 27, 2022, 10:01:38 AM »
Hello Thor,
Thanks for your response.
I use Interlink without problem.

The connection speed is very appreciable

Good day