Recent Posts

Pages: 1 ... 8 9 [10]
91
PLUS+1 Autonomous Control Library / Integrating RTK GPS
« Last post by FluidPowerTom on July 15, 2022, 05:28:37 PM »
Has anyone done or looked into integrating RTK GPS into one of these systems?  These are the very expensive centimeter-accuracy GPS solutions.
92
PLUS+1 GUIDE / Re: Certificate IEC 61508 PLUS+1 Dev Tools
« Last post by Tor on July 15, 2022, 07:00:34 AM »
Hello Niska,

Good question.
There should be a certification coming out soon if you look back to how it worked before, but I haven't heard anything. It's really quiet.
I will ask the PLUS+1 team to see if I can get any information.
As you know it's vacation time, so the answer may take some time.

Have a nice day
93
PLUS+1 Service Tool / Image repository directory not found.
« Last post by Fredrick on July 14, 2022, 07:03:41 PM »
Hi,

When trying to save a P1D file in ServiceTool 2022.2.5 I get the message  "Image repository directory not found." and if I click Yes all images that are in the P1D file disapears.
Even if I manualy add them again I will get the same question again when trying to save the P1D file.

Please se the attached picture.
94
PLUS+1 Service Tool / Re: Update Center
« Last post by Mike on July 14, 2022, 04:00:30 PM »
Perfect thanks Tor. Figured there was something simple I was missing.
95
PLUS+1 GUIDE / Certificate IEC 61508 PLUS+1 Dev Tools
« Last post by Niska on July 14, 2022, 08:45:48 AM »
Hi.

When are Danfoss coming with new certificates IEC 61508 PLUS+1 Dev Tool to ver 2022.x? So far it is still only ver 12.x that is the latest one.

BR Staffan
96
PLUS+1 Service Tool / Re: Update Center
« Last post by Tor on July 14, 2022, 06:46:53 AM »
Hello Mike,

Yes, you can save a Preset in Update Center.
When you have selected your items for you subscription, click the arrow on the "Save Changes" button and the "Save Preset" appears. If you don't chose a new item it can be hard to see, but it's there and works the same.

Have a nice day.
97
PLUS+1 Service Tool / Update Center
« Last post by Mike on July 13, 2022, 08:21:02 PM »
Is it possible to create my own preset packages for the update center?

I have picked all the files I want manually but want to create a package so anyone else using guide can just grab my presets.
98
PLUS+1 GUIDE / Re: Expanding the Drawing Area
« Last post by Mike on July 13, 2022, 08:04:09 PM »
I agree with Tom, just turn off the warning and ensure you have the "Zoom to fit graphical code" option checked.

I move my drawing completely outside of the boundary if it doesn't fit nicely, not worth the time to try to compress/nest things to fit an arbitrary scale.

Just don't go overboard writing your whole program on one page.
99
PLUS+1 CS Hardware / CS10 over VPN
« Last post by GioM on July 13, 2022, 09:22:55 AM »
Greetings,

I am currently facing issues when trying to connect a CS-10 wireless gateway through a VPN network. I read from a previous post that it's possible to achieve this connection.

-   I checked “Proxy Enabled” feature in CS-10 configuration page
-   I can correctly ping the CS-10 device from my PC through the remote local network (I assigned 192.168.100.100)

In Service Tool, I start a gateway search through “PLUS+1 Interlink” protocol (non-remote) but can’t find the device.

Could you please sort out this issue?

Service Tool Version: 2022.1

Best regards,
Gio
100
PLUS+1 Service Tool / Re: PVEA connection with the Service Tool
« Last post by G30RG3 on July 12, 2022, 07:06:38 PM »
Your screenshot included shows the panel that Danfoss has made to be used together with the hardware template in Guide, to get an overview of all checkpoints.
I think you want to use the Service tool P1D file to change the NodeId or see the data from the module itself?
These can be found @ https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-software-tools-and-applications
Pages: 1 ... 8 9 [10]