If there have been a name change for some reason, you need to open the service screens and change the signals to the correct ones. I have marked in the attached image where to look when using a regular parameter component in Service Tool. If you don't have permission/access to do this, I would recommend you to contact the developer of the service screens or the machine manufacturer.
« Last post by SVK on March 05, 2024, 01:45:35 PM »
Hi all,
I have a project file that dates from 2016. When I open it in the latest Plus+1 service tool some parameters are not shown because they don't exist or have another name. How can I fix this issue?
The parameters I haven't found yet are: EE_DOutSpd_rpm1 EE_DOutTorque_Nm3 EE_MagCurrBoost_pct2 EE_SnsrSupplyVltg EE_SpeedCalcMode EE_SpeedFOF_ms EE_VCellRst_mV SpdInvSgn Val1 To Val10
« Last post by Tor on March 05, 2024, 01:41:32 PM »
Hello,
Sorry about the late response.
I was approached by a developer who saw this topic and he wanted me to write a clarification to avoid confusion. When it comes to the DM430 and the EEPROM we guarantee 4 million write cycles.
« Last post by Lukey on February 29, 2024, 06:35:03 AM »
Hello, i am using a DM1200T.
Is there anyway to ready the 32mb applog memory size to determine how much has/is being used?
Reading the OS.RAM and OS.Flash values indicates that the applog memory usage has no influence on these values, as I cannot see an significant changes when writting/reading to the applog memory.
The Write_USB block (designed for the DP720 does not work with this hardware fully) does not give information on Used_Blocks or Free_Blocks unfortunately.
« Last post by acmall on February 26, 2024, 12:03:55 PM »
I just did a test on two projects, one using a DP720 and the other MC088-015. Both complied without issues and appear to be producing working programs on a bench test.
It would be good to find out what is causing this issue for some uses. For reference the HWD files for the programs I tested are: - MC088-015 = V200 DP720 = tested with booth V260 & V270.
This website uses cookies
We and our partners use technologies, including cookies, to collect information about you for various purposes, including:
Functionality, Statistics, Marketing
By clicking 'Accept All' you consent to all these purposes. You can also choose to indicate what purposes you will consent to using the [Check boxes], then press 'Update consent'.
You can always withdraw your consent by [clicking the small icon in the lower left corner of the page].
Detailed cookie information cannot be displayed if a cookie has been set behind a log-in webpage. However, the provided cookie consent prior to a log-in webpage is still applicable.
You can read more about our use of cookies and other technologies, as well as our collection and processing of personal data by clicking on the link.
Learn more