Author Topic: Missing Libraries  (Read 739 times)

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 310
  • Karma: +28/-1
Missing Libraries
« on: March 18, 2025, 03:34:50 PM »
Hello,

In the latest version of PLUS+1 Update Center (v1.0.183) released with PLUS+1 Tools 2025.1.2 seems to have some missing libraries and files.
We don't know why, but troubleshooting is in progress.

We are sorry for any inconvenience.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 62
  • Karma: +5/-0
Re: Missing Libraries
« Reply #1 on: March 18, 2025, 04:36:29 PM »
Hello Tor,
Thanks for this information.

I've been working with version 2025.1.2 for several days now and have had no problems.
Which libraries are affected?

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 310
  • Karma: +28/-1
Re: Missing Libraries
« Reply #2 on: March 19, 2025, 07:24:08 AM »
Hello Camox,

It shouldn't cause any issues for users with the libraries already installed in PLUS+1 GUIDE.  But if you installing GUIDE on a new PC, some libraries are not available in Update Center.
I'm not completely sure what are missing. But if I do a comparison with the libraries installed in GUIDE, everything after the Outputs Library is not shown (see image MissingLib).

Here's a tip for you Update Center users. If you don't already know it.
You can select to keep the setup files after installation. Default is to delete them.   But sometimes you need to install it again or share with a co-worker.
In Options (Tools > Options > General), make sure to deselect "Automatically delete installed files" (see image UCOptions). This will keep the setup file in the download folder.


Have a nice day.



Best regards,
Tor
PLUS+1® SW PAE Team

Offline 240glt

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +1/-0
Re: Missing Libraries
« Reply #3 on: March 19, 2025, 12:48:24 PM »
Hi Tor,

Just for your information, I could not install the new 2025.1.2 with update center. Or, the installation of Guide probably worked, but not the included update of PLUS+ Base, that was needed to run 2025.1.2. It said that I have to close update center for the installation to continue. And update center refused to be closed, since the installation of Guide is in progress...

However, thanks to your tip above, it worked when I shut down the update center and then used the downloaded installation file for Guide. (I had to do the same for service tool.)

Attached are a few screenshots of the fault, for information.
« Last Edit: March 19, 2025, 12:50:20 PM by 240glt »

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 64
  • Karma: +3/-0
Re: Missing Libraries
« Reply #4 on: March 19, 2025, 11:44:23 PM »
My update center used to show about 330 active subscriptions. Now it only shows 263.
When I installed 2025.1 an error message said I had the wrong base file and bombed out.

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 64
  • Karma: +3/-0
Re: Missing Libraries
« Reply #5 on: March 20, 2025, 11:25:50 PM »
Update center fixed now.
Base file v1.0183 fixed the installation issue.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 310
  • Karma: +28/-1
Re: Missing Libraries
« Reply #6 on: March 21, 2025, 06:52:05 AM »
Hello,

Yes. BRIan is correct. 
The Update Center issue has been be fixed by the developers.


Thank you for your patience.
« Last Edit: March 21, 2025, 06:55:21 AM by Tor »
Best regards,
Tor
PLUS+1® SW PAE Team