Author Topic: Application Log  (Read 5663 times)

Jeff Olson

  • Guest
Application Log
« on: May 03, 2011, 04:42:19 PM »
Is there a way to create a service tool button to download the app log?
We need to create a "User" tool that just downloads the log and
also has a button to erase it.

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 72
  • Karma: +0/-0
Re: Application Log
« Reply #1 on: May 18, 2011, 10:53:05 AM »
Hello,

1. Open an Advanced Parameter Function.
2. Select a Button.
3. Design the Button with a hyperlink to Read Application Log.

To erase the log you can connect a Set Pulse component to the erase function in the Applog in the GUIDE program and then use a Set Pulse object in the Advanced Parameter Function in the Service Tool.

Best regards
Stefan