Author Topic: Guide 12.1 7 Complie Break Lockup  (Read 4023 times)

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Guide 12.1 7 Complie Break Lockup
« on: July 30, 2020, 09:08:35 AM »
Has anyone experienced Guide 12.1.7 locking up if you click Break during a compile?

I have had this happen a few times on my desktop and laptop and had to kill the Guide process. Most concerning is that twice now this has resulted in the .scs file being deleted so the project was effectively lost. Fortunately I as able retrieve a recent copy so did not loose to much work?


Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: Guide 12.1 7 Complie Break Lockup
« Reply #1 on: July 30, 2020, 11:47:43 AM »
I've had the same issue today ..

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +2/-0
    • Trebro Turf Equipment
Re: Guide 12.1 7 Complie Break Lockup
« Reply #2 on: July 31, 2020, 04:24:54 PM »
I have had this issue as well. I have found that if I click break while the compile progress message is "Refreshing Project" or anything before that message GUIDE will crash. If I wait until "Refreshing project" is done it seems to break the process ok.

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Re: Guide 12.1 7 Complie Break Lockup
« Reply #3 on: August 01, 2020, 04:37:11 PM »
Yes, same issue here as well.

Offline deaks57

  • PLUS+1 Developer
  • ***
  • Posts: 24
  • Karma: +3/-0
Re: Guide 12.1 7 Complie Break Lockup
« Reply #4 on: August 02, 2020, 11:41:40 PM »
Same...

Offline tjozmin

  • PLUS+1 Developer
  • ***
  • Posts: 10
  • Karma: +0/-0
    • Oxbo International Corporation
Re: Guide 12.1 7 Complie Break Lockup
« Reply #5 on: August 05, 2020, 10:20:47 PM »
I have the same issue

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 72
  • Karma: +0/-0
Re: Guide 12.1 7 Complie Break Lockup
« Reply #6 on: August 07, 2020, 11:50:42 AM »
Hi,

This issue is reported and will be fixed as soon as possible.

Best regards
Stefan, PLUS+1 Helpdesk