PLUS+1 User Forum

PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: williamk on January 24, 2022, 11:51:08 PM

Title: File Download Failed
Post by: williamk on January 24, 2022, 11:51:08 PM
Occasionally I will get an error with the text: "Error: Download transfer timeout" and Download Status: "E266: Download transfer timeout".

Is there some way to increase the timeout?  I've seen this error while using a PEAK adapter in RP1210C mode and while using a Kvaser Leaf Light.  In both instances, the display (DM430E) and the adapter were the only things connected to the CAN bus and the bus had proper terminating resistors.
Title: Re: File Download Failed
Post by: vnikola on June 07, 2023, 09:30:28 AM
Hello!

Have you found the solution to this problem, as we are experiencing almost the same thing here.


Regards,
Nikola.
Title: Re: File Download Failed
Post by: Fredrick on June 08, 2023, 05:48:30 PM
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.

Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is buggy.
Title: Re: File Download Failed
Post by: sverreo on June 08, 2023, 09:35:36 PM
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.

Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is glitchy.

Fredrick, what do you mean CAN-King is glitchy?
Title: Re: File Download Failed
Post by: Fredrick on June 09, 2023, 04:39:47 PM
Ok, maybe I used the wrong word for it  ;)

CAN-King does not work for me, the program freezes or stops behaving normally after a while.
PCAN View always works and you can use both ServiceTool and PCAN View at the same time.

Yes, I know that you can do that with CAN-King as well if you configure it right.