PLUS+1 Software > Code sharing
J1939 DM1 and DM2 messages
(1/1)
tjozmin:
Has anyone built a block to receive engine faults? I know the EIC applications does this but I find this is mostly for a display that is dedicated to engine monitoring. The software has quite a bit of code that I have no use for.
payne.byron:
There are some blocks in the Function Library that can help with this. I as well started out using the EIC application, and then redesigned using the function blocks. Download the J1939 library here:
http://www.sauer-danfoss.com/Products/MobileElectronics/PLUS1Guide/PLUS1GuideDownloads/PLUS1FunctionBlockLiabrary/index.htm
Navigation
[0] Message Index
Go to full version