PLUS+ Tools > PLUS+1 GUIDE CANKing
Output Window
paterianus:
I used the default setup and I am connected to a S-D controller and I/O module bus and can see 20-30% bus statistics on the bar but I see nothing in the output window and no Rx,Tx statistcs, what am i missing?
Thomas:
Hi!
Have you activated any filters?
Best regards // Thomas
paterianus:
Not as far as I'm aware, used only the default template.
admin:
Hmm strange, it should work.
Please contact our helpdesk in Minneapolis for more support. We can remotely connect to your PC if possible and help you directly.
http://www.sauer-danfoss.com/Products/MobileElectronics/PLUS1Guide/PLUS1GuideSupport/index.htm
Thanks // Thomas
Jpshockster:
So I am having the same problem, I have PLUS+1 GUIDE CANKing Version 5.00.175 (BETA) on Both my laptop and desk top, the laptop shows the messages in the output window and the desktop does not. I have checked all settings and find no discrepancies, I can load .lhx form both and use service tool from both so I am confident communication is isn’t the issue. any ideas what I may be missing??
Navigation
[0] Message Index
[#] Next page
Go to full version