Recent Posts

Pages: 1 [2] 3 4 ... 10
11
PLUS+1 Service Tool / Re: Backup file service tools project
« Last post by acmall on May 30, 2023, 09:00:35 AM »
That option creates a backup of the previous saved version so you always have 2 versions, the current save and the previous save.

If you have it checked you will see an additional file with a tilde symbol in the extension like this: -
MyServiceTool.p1d
MyServiceTool.~pid
The .~pid file is the backup of the previous save. This is a normal Service Tool file, if you want to open it just rename it with a .pid extension.

A similar thing happens with the module files (.scs) in Guide except the tilde is at the start of the filename instead of the extension.
12
PLUS+1 Service Tool / Backup file service tools project
« Last post by macbahi on May 29, 2023, 11:23:36 PM »
Hello,

Please, Is't possible to have a backup of service tolls project when the Service-tools program is closing without saving project?
Some times the service tools crash and I lost all modification in the project.

I find this option in setting (see image) but I don't know what it do.

Please could you help.

With best regards
13
Telematics / Re: Group Management - working great
« Last post by Tor on May 25, 2023, 09:39:07 AM »
Hello FluidPowerTom,

Great news!!

I will forward this to the team working on this.


Thanks again and have a nice day.
14
Telematics / Group Management - working great
« Last post by FluidPowerTom on May 24, 2023, 11:21:02 PM »
I just walked a customer admin through creating a sub-group for one of their customers, creating roles, adding users, and assigning devices.  This works extremely well and easily.  That is definitely going to score us some points with this customer, so thanks all who worked on that.
15
Controllers / Re: OutputMode 3 vs 6
« Last post by Lukey on May 24, 2023, 03:31:10 AM »
The controllers are not specifically designed for industrial PLC type 0-10V output signals, check out this existing thread, FluidPowerTom gives a good example of how he has made it work.

https://www.plus1forum.danfoss.com/index.php?topic=1110.msg3527#msg3527
16
PLUS+1 GUIDE / Re: CAN communication with Siemens PLC
« Last post by Daan on May 22, 2023, 12:47:31 PM »
thank you all very much!

I'm going to dig a little deeper into everything you've given me. If I have any more questions I'll ask them here but for now I can move on.

Thanks!  ;D
17
PLUS+1 Service Tool / Lock File - Problem
« Last post by Egholm-Jonas on May 22, 2023, 10:44:42 AM »
So I have created this application, and want to protect it by locking it.
I have multiple files for downloading in my "documents folder" that I link to via different visible buttons.
So I disable "system navigator" and "menus and toolbars" in the service and application properties.
And lock the File.

BUT....
If someone with a license opens service tool and choose "Design View" and then opens the locked file.
The system navigator is visible and so is the buttons and toolbars!
And this person will then be able to download all of the files from documents folder.
The Toolkey has to be implemented in the application!
Any suggestions how to make this file locked for real?
18
Controllers / Re: OutputMode 3 vs 6
« Last post by flno on May 22, 2023, 10:27:59 AM »
Sorry, 2-10 Volt in this case
19
Controllers / Re: OutputMode 3 vs 6
« Last post by flno on May 22, 2023, 10:24:37 AM »
Year that was also my thought, that there might be some logic for more precise voltage control, but I could not see the difference in practice. My application is to generate a fixed 0-10 volt reference signal for an external embedded valve controller. Then I was wondering which output mode to choose and could not see the difference in practice.
20
General controls / Re: Electric Motors & VFDs
« Last post by swordfeather on May 19, 2023, 03:36:20 PM »
Hi,

In a project we are using the Schwarzmuller MI08 inverter.
I was not able to find the Schwarmuller hardware file on update center.
Anyone has a link for this file?

Greetings
Pages: 1 [2] 3 4 ... 10