Recent Posts

Pages: 1 2 [3] 4 5 ... 10
21
Displays / Re: Real Time Clock For DM430
« Last post by BBarry on September 08, 2022, 09:13:45 PM »
Thanks That helped a lot!!!
22
Displays / Re: Download time in DM1000
« Last post by Camox on September 07, 2022, 08:05:11 AM »
Hello Thor,
Thank a lot four your response.

I’ll get that cable fast.

Have a nice day
23
Displays / Re: Download time in DM1000
« Last post by Tor on September 07, 2022, 07:29:18 AM »
Hello Camox,

Yes the download time for the DM1x00 displays are a bit longer than the rest of units. Especially when you are replacing the HWD file and OS.
I recommend to use USB when working with the DM1x00 displays. You will save a lot of time. When it take almost an hour downloading a new OS with CG150, it will only take a minute with the USB.

If you want to order you can find the part number in the image below (11231512). You can also find it in the Data Sheet.


Have a nice day.
24
PLUS+1 GUIDE / Re: Installing V260 Display hardware files in Guide 2022.2.5
« Last post by Fredrick on September 06, 2022, 08:09:16 PM »
Works for me to to.
When I deleted the BookCase.xml file I successfully could update the HWD file for DM430E display.
25
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Fredrick on September 06, 2022, 08:07:31 PM »
Thank you for the information. :)
26
Displays / Download time in DM1000
« Last post by Camox on September 06, 2022, 04:44:15 PM »
Hello,
I work actually on software for DM1000 dysplay.
The download time for add a software in the dysplay in long. During the download the load speed on the dyspaly is 10kb/s.

We can change the load speed ?

Thank in in advance.

Good day
27
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Tor on September 06, 2022, 03:42:32 PM »
Hello,

This issue is reported (P100006351) and will be fixed in the next release.
I recommend to use the 2022.1 until this is fixed.

Sorry about the inconvenience.
28
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Fredrick on September 06, 2022, 10:57:07 AM »
Anyone else having problems with this?
Also, sometimes the P1D file does´t get saved so next time you open the P1D file the changes are lost and you now have an older P1D file without the changes you just did. :(
29
Displays / PIB - DM1x00 HWD file update
« Last post by Tor on September 02, 2022, 10:07:18 AM »
Hello,

If you have not seen the latest PIB (Product Information Bulletin) about the DM1x00 I would like to share it here.

In short:
An issue was found that can cause the device to lock and become unrecoverable. The advice is to recompile to .HWD v308 or greater for any devices with a manufacturing date of August 11 or after.
The HWDs are located in the PLUS+1 Update Center. The version stated in the Update Center is 3.8.0 for some reason, but it's v308 when installed in GUIDE.

More information in the attached image/PDF file.


Thank you.
30
Code sharing / Re: PGN 65259 SPN 588
« Last post by Matt_Eng on September 01, 2022, 08:20:10 PM »
I agree the result does seem a little strange. However, it should be possible to convert the ascii array to a string to make it easier to read.
Should just be a Retype to String, and then the checkpoint can be read in the service tool with a "String Parameter" in an advanced page.
Pages: 1 2 [3] 4 5 ... 10