Author Topic: DM430 Download problem  (Read 4509 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 113
  • Karma: +1/-0
DM430 Download problem
« on: November 16, 2021, 10:41:39 PM »
Hi!,

I work with DM430E.  I was compile and download many times.
But now I can compile but I can not download.  I had this message as follow in picture

Thanks in advance for your reply

Cordially
Mac bahi

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: DM430 Download problem
« Reply #1 on: November 17, 2021, 11:35:34 AM »
Hi macbahi,

Do you get the same issue if you compile it again and download?
It feels like the .lhx file is "corrupt"?   Also make sure you use the latest HWD. Version 150 is the latest for DM430.

If this doesn't help you please submit a case to PLUS+1 Helpdesk: https://danfoss.secure.force.com/dpscustomersupport/?product=software
Write a small description, attach the .lhx file with the problem and the project as a zip, if it's possible. If not it can be sent in later.

Thank you.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 113
  • Karma: +1/-0
Re: DM430 Download problem
« Reply #2 on: November 17, 2021, 06:02:32 PM »
Hi Tor,

In the end the problem is done without do no thing.  Maybe windows bug.

I restart guide plus one many times without effect but when I reboot my computer it's done.

Thank you very for your help

Cordially
hamid