PLUS+1 User Forum
PLUS+1 Software => Function Library => Topic started by: spittet on April 30, 2020, 04:23:13 AM
-
Hi,
I don't know if it is wanted or not, but a few symbols are missing in SVG format in the "Symbol" folder in the "Display Scalable Image Library 70112442v100" library.
I noted that at least these are missing when compared to the "000_Icon Chart.jpg" file :
- Fuel Level
- Engine Oil Pressure
- Lock
- Unlock
It would be nice if we could have access (in SVG format) to all the symbols shown in the "000_Icon Chart.jpg" file.
Addind to that, with the Tier4 / StageV requirements, I think it would be nice if you could add all the need DPF/Aftertreatment related symbols that are mandatory to be shown in a display screen. I know I can find them in the EIC program, but having these in SVG format would be easier.
Have a good day!
-
Hi,
Thanks for the information.
This library was created back in 2013 for the DP7XX displays, and I have my doubt this is updated after the EIC for the DP430 was released.
I will talk to the responsible people about this. Either they need to updated the library or maybe remove it.
Have a nice day, and stay safe.