PLUS+1 Software > Code sharing
J1939 Receiving Large Message (EC, FEE3)
PosFdbk~~~~~:
I think it is easier than that... The stuff like DM1, DM2, CI, I believe gets blasted out globally with a BAM (even if it is a PGN like DM2 or CI that must be requested with PGN 59904 RQST). I don't think you'll ever need RTS/CTS.
Anyway, you just hook up BAM to the CI and DTC parsers (Same BAM goes to multiple parsers).
For the "single packet" just hook up the generic PGN_Rx block. One each to each parser.
Through in the RQST block and you can basically do this all with existing blocks. I could probably pull together a screenshot for you if needed.
Matt_Eng:
Hi, there is actually an example included in the Update Center that shows a setup with a DM1, DM2, and a CI message being received.
It can be found under Files->Applications->PLUS+1 GUIDE examples->J1939_Example
When you download it, you'll find an scs file in the download directory that you can view and even copy.
The newer RTS_CTS + BAM setup is a little more confusing than just dropping in a DM1 or DM2 block, but in order to correctly support multi-packet messaging and satisfy J1939-82 compliance testing it was necessary.
AlbertMilani:
Hi,
I got it working using the example (PLUS+1 GUIDE examples->J1939_Example) that Matt_eng recommended! It wasn't too bad after all.
Sorry, I took so long to get back to this; I had some more urgent things to fix.
Thanks!
Albert
macbahi:
Hi!
I am interesting to see J1939 example but I didn't find it in my update center.
Please you can see my image of my Plus+1 Update center.
Thank you very much
With best regards
acmall:
Mine looks like the attached image. Update Centre version is 1.0.155.4923
Navigation
[0] Message Index
[*] Previous page
Go to full version