PLUS+1 Software > Code sharing
String Concatenate C Code POU
(1/1)
AlbertMilani:
Hi,
Does anyone have a C Code POU they could share with me that will concatenate one string to another or a POU that does something similar that could help me get started? Something that would concatenate two UINT8 arrays is probably what it should do.
I could probably do it myself but I'm sure I'd make a few dumb mistakes since I'm relatively new to GUIDE and haven't made a C Code POU yet.
Thanks,
Albert
AlbertMilani:
Well, I tried it myself and it works correctly. I'm not sure I did everything the best way; maybe someone could critique it. I was stingy with the input string length and I couldn't think of a way of relating the output string length in the code and the length specified in the VAR_OUTPUT section. I also would've liked to use pointers in the C Code but I couldn't get that to happen with the input type.
See the attachments for images of my Page and C code, and I also attached my SCS file.
Albert
Tor:
Hello,
A developer gave me this:
"To concatenate two strings natively in GUIDE, the preferred method is to use a standard ST (Structured Text) POU. (See example below)"
Code example in the P1P.
I hope it helps.
AlbertMilani:
This is much better and now I can see how to use other "STRING related PLC functions" in the GUIDE Manual.
Thanks!
Albert
AlbertMilani:
This seems to be working great except if I have any other error, I also get this warning:
--- Code: ---*** WARNING 447:1105 *** [PLC2C] PLC Code Compilation Warning {String of default length will be returned,
which may be less than expected length. Save expression into temporary variable to avoid uncertainty.}
Line: [ 1 ] in implementation of StrConcat_Native
--- End code ---
I changed the code to do what the warning recommended, 'Save expression into temporary variable to avoid uncertainty" and that warning doesn't happen anymore.
Albert
Navigation
[0] Message Index
Go to full version