PLUS+1 User Forum

PLUS+1 Hardware => Controllers => Topic started by: macbahi on February 01, 2024, 03:28:48 PM

Title: Can isolation
Post by: macbahi on February 01, 2024, 03:28:48 PM
Hello all,

I use module SC050, OX024, DM430 and engine
I want to use Can_0 communication only between SC050 and engine.
And use Can_1 communication with SC050, OX024 and DM430.
I think for module OX024 it's ok.  It's done Please see image enclosed.
But I don't know if I must to change also Can_0 of DM430 and SC050 secondary to Can_1.
Or just connecting modules to Can_Bus_1.
Specially SC050 secondary.

I hope you understand my idea.

Thanks in advance for you help

With best regards
Mac bahi

Title: Re: Can isolation
Post by: mtrbib on February 02, 2024, 03:47:21 PM
Hello 8)

SC050:
- For the engine communicatione you need to use CAN0 (CAN port 0)
- For the OX024 and DM430 CAN1 (CAN port 1)

DM430:
- CAN0 (if you are using the physical CAN0)

OX024:
-CAN0
Title: Re: Can isolation
Post by: macbahi on February 05, 2024, 11:20:01 PM
Hello mtrbib

thanks

with best regards