PLUS+1 Hardware > Controllers
where can I find compiling error notes explained?
(1/1)
bship:
I am trying to compile a test program and the error comes up - *** ERROR 23 *** [chpargu1] NOTHING CONNECTED ON COMPONENT: {Hardware Output}, ENTRY A1
MC50_10T_MC50_12T!TOP!Outputs!C1p31_DigOut!C1p31 (228,142)
1. What does this mean, I think my lines are all connected?
2. Where can I find an index of error message explanations?
Thanks
hproffitt:
It means that pin 31 is not seeing a connection. It has to have a constant T or F on it, or be connected to logic elsewhere in the program to supply the T/F to it. If you go to "OUTPUTS", then the "PIN 31" page, you can do a 'view net' or trace the logic by hitting "v" and clicking on the wire.
bship:
Thanks, I traced it back to my pages connection to the outputs page
Navigation
[0] Message Index
Go to full version