Author Topic: How does the Service Tool 7.1 pick what controller to download  (Read 4303 times)

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
How does the Service Tool 7.1 pick what controller to download
« on: December 17, 2014, 02:26:50 PM »
I've been playing around with the new Service Tool a little and I like that the service tool is able to choose what controller to download a program into. 

Then I was wondering what happens if I have multiples of the same controller on a system, such as 2 MC088-015 controllers.  How does the service tool choose which controller to use then? 

I have a system that has a node address of 1 and the other has a node address of 9.  I created a simple program that has a node address of 7 to see what controller it would choose for download and it chose the controller with an address of 9.  What if I wanted to over ride the program that was in the controller at address 1?  As far as I can tell, it does not allow me a choice between the two controllers.

What logic does the service tool use in choosing a controller for program download?

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Re: How does the Service Tool 7.1 pick what controller to download
« Reply #1 on: December 17, 2014, 03:10:53 PM »
Never mind, I just found out that the ECU box is actually a pull down box.