Author Topic: DM1000 does not start  (Read 1946 times)

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
DM1000 does not start
« on: September 23, 2022, 12:12:45 PM »
Hello,
I work with an DM1000 on my desk with a 24v power supply.
Today, the screen does not start. I verify the supply is good on C1P1 and C1P2.

I went through the documentation but I can’t find anything to check or test.
Do you have any idea?

Thank in advance.
Good day

Offline mtrbib

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
Re: DM1000 does not start
« Reply #1 on: September 23, 2022, 01:42:31 PM »
Hi,

Did you check if you are working with the newest HWD?

Can you still connect to it with the ServiceTool?

Best regards

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
Re: DM1000 does not start
« Reply #2 on: September 24, 2022, 08:20:08 AM »
Hello,
Thanks four your response.
Ican't connect to the dysplay with the service tool.
I had updated the hardware file three weeks ago.

Thanks

Offline deaks57

  • PLUS+1 Developer
  • ***
  • Posts: 24
  • Karma: +3/-0
Re: DM1000 does not start
« Reply #3 on: September 26, 2022, 12:39:22 AM »
Contact Danfoss. There is a way to fix this.

Offline ramzilla

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: DM1000 does not start
« Reply #4 on: October 10, 2022, 05:35:10 PM »
I had to add a switch on the power wire in order to get a DM1000 to power up with a desktop power supply. Turning on the power supply would not power up the display. I have to turn on the power supply and then flip the switch to get it to come on.

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 36
  • Karma: +2/-0
Re: DM1000 does not start
« Reply #5 on: October 12, 2022, 11:48:19 AM »
Yes. Thanks.
I think is this problem.
I have also a mystake with my wire.