Recent Posts

Pages: [1] 2 3 ... 10
1
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Tor on Today at 01:59:54 PM »
Hello,

Yes I see the same thing.  I will report this.


Thanks for letting us know.
2
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Fredrick on October 01, 2022, 05:15:33 PM »
ServiceTool 2022.2.6 fixed the issue with the "Image repository directory not found." when using "File/Save As" in ServiceTool
But the problem is still present when importing some PFX files in ServiceTool, I get the same error message after I have imported a PFX file into the Tool and then trys to save.

In 2022.1 it works when I try to do the same action.
3
Displays / Re: DM1000 ImageViewer GIF support
« Last post by Matt_Eng on September 28, 2022, 03:05:44 PM »
There is a one way to have a GIF like animation, but it is a little clunky. I've used it to have a simple little pixel fire animation on my DM430.
Step 1. Extract the individual frames of the GIF file using a tool, I just used an online one.
Step 2. Create an image list in the screen editor project library, add the individual frames to a sub folder, and then edit the image list to include the frames from the sub folder.
Step 3. Add the Image list to the screen area and then set the ActiveIndex property to an input signal.
Step 4. Add an oscillator and a counter to increment the ActiveIndex of the list every x milliseconds, mine was every 40ms, some of the frame split tools will tell you what the delay is.

-Matt_Eng
4
Displays / Re: DM1000 ImageViewer GIF support
« Last post by Tor on September 27, 2022, 03:34:02 PM »
Hello,

After talking to people who should know and done some tests I can confirm that "Animated" GIFs are not supported.

Sorry.
5
Displays / DM1000 ImageViewer GIF support
« Last post by CatEclipse on September 27, 2022, 12:42:40 PM »
Hi,

I have tried uploading a GIF to DM1000 display using the functionality ImageViewer.
It is specified there that GIF is a supported format.
However, on the screen it shows the GIF I have uploaded but it is not animated. Just static one frame picture.
So it is actually not supported for dynamic animations?
Is the only way to upload a dynamic picture, is to have a video and use media player?
Thanks!
6
PLUS+1 Service Tool / Re: Conditional Hide Page
« Last post by acmall on September 27, 2022, 09:48:54 AM »
Thanks for confirming Tor.

7
PLUS+1 Service Tool / Re: Conditional Hide Page
« Last post by Tor on September 27, 2022, 09:12:21 AM »
Hello acmall,

Unfortunate no.
The closest thing is to use the hide functionality on a Panel component. This will still leave an empty page in your Parameter Page tree, but you only need to do the hide setting on one component, not 50.

This wish is already in the wishlist, so there might be a solution in the future.


Have a nice day.
8
PLUS+1 Service Tool / Conditional Hide Page
« Last post by acmall on September 26, 2022, 06:28:14 PM »
Does anyone know if it is possible to hide a log or parameter page based on a condition in a similar way to setting a hide condition for the visibility of a component? The only option I can see is Hide in Run Application Mode.

I was about to post it as a suggestion but thought I would check here first in case I am just missing it!
9
Displays / Re: DM1000 does not start
« Last post by deaks57 on September 26, 2022, 12:39:22 AM »
Contact Danfoss. There is a way to fix this.
10
Displays / Re: DM1000 does not start
« Last post by Camox on September 24, 2022, 08:20:08 AM »
Hello,
Thanks four your response.
Ican't connect to the dysplay with the service tool.
I had updated the hardware file three weeks ago.

Thanks
Pages: [1] 2 3 ... 10