Author Topic: Lifetime NVmem Erase/Write for DM430E  (Read 3242 times)

Offline JHansonHere

  • PLUS+1 User
  • **
  • Posts: 6
  • Karma: +0/-0
Lifetime NVmem Erase/Write for DM430E
« on: October 18, 2023, 05:36:50 AM »
I can't find anything on the Non-volatile memory other than it having a 32kB EEPROM. Anyone know the lifetime erase/write cycle number for these?

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Lifetime NVmem Erase/Write for DM430E
« Reply #1 on: November 29, 2023, 04:12:54 PM »
Normally this EEproms are ferromagnetic and so millions of erase/write cycles.
I just find no document, sorry.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline samuelhj

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: Lifetime NVmem Erase/Write for DM430E
« Reply #2 on: December 18, 2023, 02:30:40 AM »
I'm doing quite a bit of an educated guesses here from my limited experience with the DM430, but they seem to use STM32F777 series and their flash cycle per datasheet is about 10k cycles if my memory serves right, however they could be using an external NVRAM for data storage which would make it a bit impossible to guess unless just opening one of those displayes and look at the hardware inside. What I believe plus1 is doing is writing stored values to EEPROM which has ~100k write cycles (or at least that's how I'd do it).

The better question is, why would you need to write so often to a flash memory or eeprom that this is a question, unless for pure education purposes. (I also assumes plus1 is doing something in the background to preserve flash or eeprom memory, or at least they should).

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Lifetime NVmem Erase/Write for DM430E
« Reply #3 on: December 18, 2023, 12:51:36 PM »
Here it is DP570, but it is the same technique:

"FRAM Memory
DP570 Series Displays use Ferroelectric Random Access Memory (FRAM). FRAM has a write endurance of
over 100 trillion cycles, which is ideal for datalogging. 2kB is available for application."
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Lifetime NVmem Erase/Write for DM430E
« Reply #4 on: March 05, 2024, 01:41:32 PM »
Hello,

Sorry about the late response.

I was approached by a developer who saw this topic and he wanted me to write a clarification to avoid confusion.
When it comes to the DM430 and the EEPROM we guarantee 4 million write cycles.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team