PLUS+1 Hardware > PLUS+1 Compliant Hardware

JS6000 & JS7000 CAN Function Block TimeOut Output

(1/1)

acmall:
The CAN receive function blocks for the JS6000 & JS7000 have two signals TimeOutBJM and TimeOutEJM.

The user manual for the CAN function blocks state that these signals indicate if the function block receives the respective messages within a 100ms timeout limit (T = Message not received within 100ms limit, F = Message received within 100ms limit).

I am having an issue with these blocks as both are not indicating the timeout unless they have received at least one message. Is anyone else seeing this?

Navigation

[0] Message Index

Go to full version