Recent Posts

Pages: 1 2 [3] 4 5 ... 10
21
Displays / Re: QT in Guide
« Last post by Tor on September 05, 2024, 10:57:54 AM »
Hello acmall,

I have reached out to the responsible persons regarding your question and I'll post here as soon as I get a response.


Have a nice day.
22
Displays / Re: Export image library for old project
« Last post by Camox on September 04, 2024, 09:55:47 AM »
Thanks you for your response.
In video, the function used is "Export Screen Definitions". But this function is unavailable in old project.

Am I wrong?
23
Displays / QT in Guide
« Last post by acmall on September 04, 2024, 09:04:02 AM »
@Tor mentioned QT in another thread so wanted to ask is this how Danfoss is planning to add screen functionality that has been requested for many years and catching up with what is available in other well known programming systems or do they have plans to offer Guide native solutions to improve the screen functionality?

I am not familiar with QT but looking at the website it requires a €2140 per year subscription.
24
Displays / Re: Export image library for old project
« Last post by Tor on September 04, 2024, 08:03:38 AM »
Hello Camox,

I'm sorry, there is no easy "Export Images" as for the texts.

This YouTube video might give you some hints on the workflow to transfer display projects from one display to another.
https://youtu.be/iPJ9rvlGnDg?si=j1he5R9rCfBR99OZ

With the introduction of QT in PLUS+1, transfer display project will probably be easier in the future.

Have a nice day.
25
Communication / Multiple Computer connections via WIFI With Service tool
« Last post by Mike AA on September 03, 2024, 07:02:08 PM »
I have a Trencher that is curerently being monitored nearby with a laptop for QC. Essentially they are watching what 6 different sensors are reading. If I want to pull a machine log or monitor more items not shows on the other laptop on my programming laptop I get an error about multiple connections and must put the other laptop in offline mode. This machine has 2 DS1200 with WiFi, I don't recall if it was giving me the error if I connected to the separate displays but I feel it was a CANBUS network error kinda thing.

Has anyone else tried to connect to a Plus+1 component using two different connections? I will try again here in a moment to see what the error it throws is and give more info.

I like pushing the limits of this hardware and software.

Thanks,
Mike
26
Displays / Export image library for old project
« Last post by Camox on September 03, 2024, 04:44:12 PM »
Hello,
I'm in the process of reworking an old DP600 screen project.
When I copy my screen definitions, the image and text libraries are not copied.
I have found a way to export the text definitions from my old project and import them into my new project.
But I can't do it for the images. There are no import and export methods available for images and pasting images doesn't work.

Do you have a solution?

Thanks in advance
27
Hello mfor,

This error seems to appear when a WMI repository file within Windows is corrupted.
This should be a situation where onsite IT personnel should have the knowledge to reobtain this file.
There have been multiple confirmations from customers that their IT department was able to restore/rebuild the WMI repository and everything was working again.

I'm sorry, but this is all information I have.


Have a nice day.
28
Hello All,

I recently installed Update Center to install Plus+1, but anytime I try to start it, I get a Command Prompt popup that briefly states, "Exception EOleException in module P1UpdateCenter.exe at 00114BAB. Invalid class.", then disappears.

Are there any fixes for this? Thank you for your time.
29
Displays / Re: Read Extracted AppLog
« Last post by Lukey on August 21, 2024, 06:16:04 AM »
What kind of applog data manipulation are you running/processing/doing?

I would look into Excel Scripts/Macros or VBA Macros to streamline your data manipulation if you are repeating the same processes.

Also once you have that formula/process for the data manipulation defined you could build an executable file that would auto complete your post processing requirements.
30
Displays / Read Extracted AppLog
« Last post by QWERTY on August 20, 2024, 08:45:31 PM »
Hello, I have a DM1200 Display and I recently started to use the AppLog. It can go up to 32 MB. When we extract it from the screen, we get an Excel Sheet with all the data from top to bottom. This sheet will have up to 900 000 rows when the 32 MB of the display is full. And all of those rows are one on top of the others, which is not easily readable. I started sorting the data within Excel but loading times are far too long because of the amount of data.

I wanted to know how do you go from the raw AppLog file to a more readable and friendly sheet, without having to much loading time. Do you guys stay within excel or do you extract the data elsewhere? Or maybe you have other technique that I am not aware of.
Pages: 1 2 [3] 4 5 ... 10