PLUS+1 Hardware > Controllers

use MC50 and IOX24 together

(1/3) > >>

topal:
Hello,

I would need to know if when using an IOX24 module with an MC50-110n controller it is mandatory to use the SUB-CMDs of the IOX24 module for my program which is in my MC50 or else I can directly use the name of the IOX24 input?

because when I use the name of the inputs directly it does not work

and when I want to use SUB-CMd it's me who doesn't understand how to use these commands

could you help me ?

thank you

Pat

Marbek_Elektronik:
Here an example:

Marbek_Elektronik:
and this

Marbek_Elektronik:
(Perhaps you find a newer document)

The can_config of Module is important:
In example I have NodeID=0

Marbek_Elektronik:
See here

Navigation

[0] Message Index

[#] Next page

Go to full version