PLUS+1 Software > Code sharing
Project creating help needed.
(1/1)
Wireloom OY:
Hello,
Our company is new user of Plus+1 Guide and Danfoss hydraulic components.
We need to build up project for our forest crane operating for Danfoss valves. We use 2 PROF1 yoystics + MC024 controller + 8 PVEA actuators.
I am beginner on programming field. I passed free e-learning courses.
I already started with project but need somebody to assist me to look project over and help to find weak points.
With best regards,
Kristjan
FluidPowerTom:
I really haven't got time to look anything over, but I can offer some advice. First, I recommend going through the tutorials in the GUIDE user manual starting on page 502. The e-learned, sadly, is very much outdated in many ways.
Next, use the Service Tool to monitor input from your joystick (CAN or no?). If it is a CAN joystick then you'll want to get the Compliance block for it to make it easier to pick up the X and Y axis. Then you'll want to get the Compliance block for the PVEA actuator. These compliance blocks have a user manual that you'll want to at least skim. Also the technical manual for your PVEA will indicate how to wire it and what sort of signal it needs (10% to 90% of battery voltage I think). Following all that, see if you can get one joystick axis to drive one PVEA and go from there.
Wireloom OY:
Hello Tom,
Thank You very much for You time to give advice.
Yes we use CAN joysticks. I will go through the manual, go forward with blocks and try to get first actions to move.
With best regards,
Kristjan
Navigation
[0] Message Index
Go to full version