PLUS+1 Software > Communication
Error 74 attempting to define an RS232 message on DP710
(1/1)
bfpmark:
*** ERROR 74 *** [GLINK] NO ARRAY DECLARATION OF SIGNAL: {UART[0].TxMsg.Data[1]}, FILE: {DP710T.exr}
What does the above error mean, and how do I resolve it.
I've used the following two Hardware Definitions and neither seems to work:
UART[0].TxMsg.Data[0]
UART[0].TxMsg[1].Data[1]
Based on the API, the first one should work. Any advice would be appreciated.
Marbek_Elektronik:
Looking to my DP610 TX-routine:
UART[0].TxMsg[0].Data[0]
UART[0].TxMsg[0].Data[1]
UART[0].TxMsg[0].Data[x]
bfpmark:
Turns out the solution on the dp710 is:
UART[0].TxMsg.Data
but you have to connect a signal that represents an array[241].
The 241 sized array is processed as one signal, where as in the DP6xx, you had to use 231 lines to receive it.
Navigation
[0] Message Index
Go to full version