I can speak for Hawe valves:
ReqFreq: default 4000Hz
PinConfig: 5
Maximum current 1100mA
Dither frequenc 100Hz
CurChgLim: default 111
Dither amplitude 100mA
For all valves an all dirctions the same parameters.
Sorry to dig up an old thread from 2015/2016.... I can create a new topic/thread if necessary.....
I am running into some Dither related questions, specifically on a HAWE valve. Mainly it is the Slew/Swing valve of a crane. 24V system. At first I was not using dither, and the control was not so precise. Adding dither has helped, but it still isn't perfect. I am trying to narrow down the right values for the Output Config.
Marbek_Elektronik..... I am essentially using the values you mentioned. However you mentioned a Dither amplitude of 100mA. Is that a value of DitherAmp=100, which is actually 10.0mA since the unit is 0.1mA? Or DitherAmp=1000 which is actually 100.0mA? I have tried both ways....
-Input value of 100, corresponding to 10.0mA, and it works fairly well.
-Input value of 1000, corresponding to 100.0mA, and it the movements seem very jumpy/jerky.
(I left it at 10.0mA for now)
Another thing I am noticing..... is this normal?
-When moving the joystick from Neutral to 1% (min), it commands 230mA to the valve, and it is a nice slow movement.
-However if I "slowdown" from max speed (100% joystick) down to the same 1% (min), command is back to the same 230mA, but the movement is noticeably faster (when compared to neutral to min).