Recent Posts

Pages: [1] 2 3 ... 10
1
Code sharing / Re: String Concatenate C Code POU
« Last post by AlbertMilani on Today at 03:24:37 AM »
This seems to be working great except if I have any other error, I also get this warning:
Code: [Select]
*** WARNING 447:1105 *** [PLC2C] PLC Code Compilation Warning {String of default length will be returned,
which may be less than expected length. Save expression into temporary variable to avoid uncertainty.}
Line: [ 1 ] in implementation of StrConcat_Native

I changed the code to do what the warning recommended, 'Save expression into temporary variable to avoid uncertainty" and that warning doesn't happen anymore.

Albert
2
PLUS+1 Service Tool / Re: Looking for connecting to PVED-CC Serie 4
« Last post by Stephane on January 23, 2023, 09:45:13 AM »
Thank you very much, i found the PVED S4. Great!
3
PLUS+1 Service Tool / Re: Looking for connecting to PVED-CC Serie 4
« Last post by FluidPowerTom on January 20, 2023, 06:09:30 PM »
You'll want to use the PLUS+1 Update Center and find it in there.  I also look on the website first often times, and when I can't find it there the Helpdesk always says to use the Update Center software to find it.  The Update Center comes with the GUIDE platform.
4
Controllers / Re: SC050 examples
« Last post by macbahi on January 20, 2023, 03:12:51 PM »
Hello Tor

Thank you very much sir.

It's a shame because I thought the controller was redundant.

Now please if an output is enabled on the primary but I don't want it to be conditioned on the secondary. I can do False DisableOutput. If there is a problem, can the primary do its safety job despite the secondary output Disableoutput being forced to False.

Please my last question: is it possible to do the test. In other words, how to be convinced that SIL2 is done.

Thanks
Cordially
5
Controllers / Re: SC050 examples
« Last post by Tor on January 20, 2023, 07:10:28 AM »
Hello,

No, you cannot use the secondary processor as a redundant unit if the first one breaks down. If you look at the template for the secondary you only have "DisableOutput" as a signal out.
What you can do is to have your own code in the secondary processor to monitor specific safety functions that can shut down the output.  But again, I recommend you to read the safety manual before doing so.

Have a nice day.
6
Controllers / Re: SC050 examples
« Last post by macbahi on January 19, 2023, 11:39:05 PM »
Hello Tor,

Thank you very much for your information:
The secondary processor is there to check that the first processor is working correct (to achieve SIL2) and shut down the outputs if it's not. This is already done in the background, without you adding any logic.

But please If I want use the secondary as redundant processor, Is it possible to do that?
As example if there is any problem with an output in the primary processor, normally the controller will switch to the secondary processor to keep the output available.

Thanks in advance for your help

With best regards
7
PLUS+1 Service Tool / Looking for connecting to PVED-CC Serie 4
« Last post by Stephane on January 19, 2023, 04:53:42 PM »
Hello,

I want to connect to a valve PVED-SS Serie 4
Accordinf to the pdf, i must download the PLUS+1 PVE Service tool S4 DJ ref 11103046.
But i can't find it on danfoss.com

I download the PLUS+1 Service Tool 2022.4.
But i was only able to download the p1d file for the PVED-CC serie 5.

Is there any solution?

Best regards.
8
Off topic / Con Expo 2023
« Last post by FluidPowerTom on January 18, 2023, 06:20:56 PM »
Will a goodly chunk of Danfoss PLUS+1 / Electronics people be at Con Expo this year?  I know we've got some pretty big (for us) PLUS1 customers with booths there that I'll be connecting with, but I wouldn't mind connecting with some Danfoss folks as well.  Feel free to send me a PM if you want to get together.  Personally, I'll just be there 3/16 and leaving 3/18.
9
General controls / Re: Set Pulse by Service tool
« Last post by Camox on January 17, 2023, 09:28:48 AM »
Hello,
Thanks for your response.
I make test. The SetPulse component is only available in advanced page.

Good day
10
PLUS+1 Compliant Hardware / Re: Using Sensor_3Pt with Joystick JS6000
« Last post by macbahi on January 17, 2023, 05:04:46 AM »
Hello

Here is calculation detail see picture.

From those calculates I think the range and unit of sensor_3Pt are 10000 and 0.01.

Both real and calculate result are the same.

With bests regards 
Pages: [1] 2 3 ... 10