Author Topic: Two PVEs on a single OX24-110 pin  (Read 16373 times)

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +4/-0
Two PVEs on a single OX24-110 pin
« on: November 13, 2024, 12:16:08 PM »
Hello,
We need to add functionality to a second-hand machine equipped with an OX24-110 module.
The number of outputs available to control a PVE coil is insufficient.
I'd like to know if it's possible to control two PVE coils simultaneously with a single output. Have you ever done this?

Thanks in advance.

Offline Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 73
  • Karma: +8/-0
Re: Two PVEs on a single OX24-110 pin
« Reply #1 on: November 13, 2024, 02:08:18 PM »
PVE Ratiometric coils?
I have not physically tried it but in theory it should work just fine, the output from the expansion module is only a reference voltage to the coil/s, there is no load, there shouldn't be an issue.

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +4/-0
Re: Two PVEs on a single OX24-110 pin
« Reply #2 on: November 13, 2024, 02:41:35 PM »
We use active PVEA.
Thanks

Offline Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 73
  • Karma: +8/-0
Re: Two PVEs on a single OX24-110 pin
« Reply #3 on: November 14, 2024, 01:08:08 AM »
PVEA is Ratiometric yes, therefor I would bet Yes it should work fine with two coils on 1 output.

Regarding Active feedback or passive that shouldn't be a concern as is only related to the Fault Output of the PVE to Input of Controller.

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +4/-0
Re: Two PVEs on a single OX24-110 pin
« Reply #4 on: November 14, 2024, 08:45:11 AM »
Thank you for your answers.
Have a nice day!