Author Topic: CANopen Service screen  (Read 4988 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
CANopen Service screen
« on: December 30, 2020, 04:20:37 PM »
hey Guys,

does anyone knows how to download the CANopen service screen service tool files so that it can be use?

the one that comes along with the function blocks for CANopen.

I tried to save it but it just does not work, double click neither work




Offline mtrbib

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
Re: CANopen Service screen
« Reply #1 on: January 04, 2021, 11:27:59 AM »
Hey pinias

Did you try to save the File and then import it in to a ServiceTool file?
« Last Edit: January 04, 2021, 01:40:59 PM by mtrbib »

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: CANopen Service screen
« Reply #2 on: January 04, 2021, 02:48:42 PM »
Hey mtrbib,

that is the thing, when you try to save it, it does not choose any file extension like p1d. so it is just not recognized by the service tool.

Regards

Offline mtrbib

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
Re: CANopen Service screen
« Reply #3 on: January 04, 2021, 03:10:20 PM »
Well the filetype is given by the .pfx

Try to add .pfx to the filename

It works fine for me.

1. Save As..
2. Open ServiceTool
3. Make a new file
4. Right click on Parameter Pages and then Import...
5. Select the saved Page
« Last Edit: January 04, 2021, 03:14:00 PM by mtrbib »

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: CANopen Service screen
« Reply #4 on: January 04, 2021, 04:07:28 PM »
Hey mtrbib,

that did work, thanks for the help.

interesting, for non programable hardware it gives you the P1d file directly.

thanks again

Regards

Offline G30RG3

  • PLUS+1 Expert
  • ****
  • Posts: 71
  • Karma: +3/-0
Re: CANopen Service screen
« Reply #5 on: February 13, 2021, 08:13:22 PM »
Just like that, Danfoss released Guide v12.2.9 that doesn't like to save files anymore...  it overwrites the extension by .* and gives an error.

In V12.1.8 works correct.