PLUS+1 User Forum

PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: Fredrick on November 16, 2022, 07:43:06 PM

Title: WARNING! Service Tool 2022.3.7
Post by: Fredrick on November 16, 2022, 07:43:06 PM
Hi, I just downloaded the latest ServiceTool and it has a serious and dangerous bug when importing parameter files, see attached pictures for an example.

The parameters "Transport_Page1_Enable" and "Transport_Page10_Enable" are Booleans but when I import the parameters into the parameter list in the latest ServiceTool it looks like the values from "Transport_Hinge_Flow_A" and "Transport_Hinge_Flow_B" is used instead of the actual values in the XML file.  :o

Same happens with other parameters in the list as well.
Title: Re: WARNING! Service Tool 2022.3.7
Post by: Tor on November 17, 2022, 08:04:37 AM
Hello,

I talked to the PLUS+1 Service Tool developers and found out that you are correct. There is an issue with importing XML files.
As far as I understood, the problem occurs when there is a difference between the XML list you import and the parameter list in the Service Tool. I don't have any more details.

My recommendation is to use the 2022.2 version until this is fixed.

Sorry about any inconvenience.

Title: Re: WARNING! Service Tool 2022.3.7
Post by: Tor on November 29, 2022, 07:23:16 AM
Hello,

There's a new version of the PLUS+1 Service Tool, v2022.3.8, released in the Update Center.

Image from the release notes.


Have a nice day.
Title: Re: WARNING! Service Tool 2022.3.7
Post by: Fredrick on December 12, 2022, 08:51:10 PM
Thanks, now it works well.
The new ServiceTool also appears faster then 2022.2, specially when it comes to downloading parameters.