Author Topic: Image repository directory not found.  (Read 3909 times)

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Image repository directory not found.
« on: July 14, 2022, 07:03:41 PM »
Hi,

When trying to save a P1D file in ServiceTool 2022.2.5 I get the message  "Image repository directory not found." and if I click Yes all images that are in the P1D file disapears.
Even if I manualy add them again I will get the same question again when trying to save the P1D file.

Please se the attached picture.

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Re: Image repository directory not found.
« Reply #1 on: September 06, 2022, 10:57:07 AM »
Anyone else having problems with this?
Also, sometimes the P1D file does´t get saved so next time you open the P1D file the changes are lost and you now have an older P1D file without the changes you just did. :(

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Image repository directory not found.
« Reply #2 on: September 06, 2022, 03:42:32 PM »
Hello,

This issue is reported (P100006351) and will be fixed in the next release.
I recommend to use the 2022.1 until this is fixed.

Sorry about the inconvenience.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Re: Image repository directory not found.
« Reply #3 on: September 06, 2022, 08:07:31 PM »
Thank you for the information. :)

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Re: Image repository directory not found.
« Reply #4 on: October 01, 2022, 05:15:33 PM »
ServiceTool 2022.2.6 fixed the issue with the "Image repository directory not found." when using "File/Save As" in ServiceTool
But the problem is still present when importing some PFX files in ServiceTool, I get the same error message after I have imported a PFX file into the Tool and then trys to save.

In 2022.1 it works when I try to do the same action.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Image repository directory not found.
« Reply #5 on: October 03, 2022, 01:59:54 PM »
Hello,

Yes I see the same thing.  I will report this.


Thanks for letting us know.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Re: Image repository directory not found.
« Reply #6 on: December 27, 2022, 03:39:46 PM »
Hi,

Is there any new information or a workaround on the problem with importing .PFX files?
Sometimes it´s works without the problem with Image repository and sometimes not, In ServiceTool 2022.3.8 I also got a new error message while trying to import a .PFX (see screenshot).


Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Image repository directory not found.
« Reply #7 on: December 28, 2022, 10:18:55 AM »
Hello Fredrick,

Can you please add a case to the PLUS+1 Helpdesk: https://danfoss.my.salesforce-sites.com/dpscustomersupport/?product=software
Please add the information you wrote here and also mention the report number: P100006413.

According to the report this should have been fixed in v2022.3.8.


Thank you
Best regards,
Tor
PLUS+1® SW PAE Team