Recent Posts

Pages: [1] 2 3 ... 10
1
PLUS+1 CS Hardware / New CS10 videos
« Last post by Tor on December 02, 2022, 11:16:03 AM »
Hello,

We have some new released YouTube videos for the CS10.

Set up WiFi Connection: https://youtu.be/fV2DmM28Pro
Set up Bluetooth Connection: https://youtu.be/_-E7TahNRzI
Set up M2M Connection: https://youtu.be/K81Wo_aqMAE

I hope they can be useful for you.

Have a nice day.
2
Displays / Re: Real Time Clock For DM430
« Last post by Tor on December 01, 2022, 08:00:50 AM »
Hello,

You can see what HWD you have in the Project manager, (#1 in the image).
If it's not 170, go to the Update Center and make sure you have that unit selected in your subscription (#2 in the image).
When you have selected that you'll get these notifications in the Update Center (#3 in the image) when there's a new HWD. Also, the HWD text in GUIDE will turn read if there is a new HWD file you subscribe on.

If the HWD is fine, I guess you have an issue with the logic. The image you posted doesn't show much.
In the second image is my small test logic for the RTC.

I hope it can help.

3
Displays / Re: Real Time Clock For DM430
« Last post by BBarry on December 01, 2022, 02:50:11 AM »
Thanks Tor for the quick response.

I did that and it did not work.

Where can I check to see if I have the latest HWD file?
4
Displays / Re: Real Time Clock For DM430
« Last post by Tor on November 30, 2022, 12:13:17 PM »
Hi,

- Set "Stop" to On
- Change the values for time and date. (Download if you are using NV memory from ST)
- Toggle "Set" (On and Off)
- Set "Stop" to Off

Now the clock should be updated and running.  At least this is the way I did it in my test.
Also check that you are using the latest HWD file.
5
Displays / Re: Real Time Clock For DM430
« Last post by BBarry on November 30, 2022, 03:56:12 AM »
Hello all,
I am still having trouble. I believe I am doing everything needed. I set the stop bit - wait 1s. The turn the set on for a scan. Turn the set off. Wait one second before turning the stop back on again but the values are not being set. They are not even being set to zero. RTCStatus is zero thru the entire process.

Attached image - any advice?
6
PLUS+1 Service Tool / Re: WARNING! Service Tool 2022.3.7
« Last post by Tor on November 29, 2022, 07:23:16 AM »
Hello,

There's a new version of the PLUS+1 Service Tool, v2022.3.8, released in the Update Center.

Image from the release notes.


Have a nice day.
7
PLUS+1 News / Re: Developer's Conference 2023
« Last post by FluidPowerTom on November 28, 2022, 06:24:08 PM »
Thanks for the update Tor.  Fortunately, both Todd and I are on that team, so we'll make sure to fast track the proposal.
8
PLUS+1 News / Re: Developer's Conference 2023
« Last post by Tor on November 28, 2022, 03:25:50 PM »
Hello,

Sorry about the late response but getting information about this is not easy.
The only thing I have managed to find is that work is being done on a proposal that will be presented to the Leadership Team. But the road from that to a conference is long.

I wish I could give you better/more information, but I will get back to you as soon as I hear anything.


Have a nice day.
9
Controllers / Re: SC050-020 Digital Out Errors
« Last post by macbahi on November 25, 2022, 05:20:33 PM »
Hi all,

I have the same problem with SC024. I use C2P07 as Dig output to power Coil.
After a few cycles of the digital output turning off and on, the output stooped working and requires power cycle to reset controller.

I want to use the solution proposed here in this topic but I can not found  "DisableOutputSafetyMonitoring".

With best regards
10
PLUS+1 GUIDE / Re: Certificate IEC 61508 PLUS+1 Dev Tools
« Last post by Tor on November 25, 2022, 11:05:22 AM »
Hello,

Unfortunately, it's not up to Danfoss at this point.

Danfoss is still waiting for the company that performs the certification (RISE) to answer when they expect to have a certificate ready.
They had a few questions earlier this month, but it was clarified by the responsible team within Danfoss.

I'm sorry I didn't have a better answer to you.

Have a nice day.
Pages: [1] 2 3 ... 10